• No : 44477
  • Release Date : 2024/07/02 19:06
  • Print

Regarding Selecting a mapping pattern for PDO communication

There are four mapping patterns (TPDO, PRDO) for PDO communication in GX Works3. Which one should I select in FX5-CCLGN-MS?
Category : 

Answer

On the FX5-CCLGN-MS, select "3rd Transmit PDO Mapping" and "3rd Revive PDO Mapping."
The 3rd mapping pattern corresponds to the profile position mode (pp), profile speed mode (pv), profile torque mode (pt) and homing mode (hm) of the CiA402 control modes.
 
The 1st, 2nd, and 4th mapping patterns are not supported.
 
See the manual below.
MELSEC iQ-F FX5 CC-Link IE TSN Master/Local Module User's Manual
Product Name
FX5-CCLGN-MS
Product Category
Network/Communication
Series
MELSEC iQ-F Series