The maximum number of servo amplifiers connected to the FX5-CCLGN-MS varies according to the number of axes.
Example: When connecting a 3-axis servo amplifier, the FX5-CCLGN-MS can connect up to 20 stations when the maximum number of connected stations is 60/the number of axes is 3.