• No : 44607
  • Release Date : 2024/11/28 16:12
  • Print

Regarding Error code H1968 of FX5-ENET Mail send FB

Error code: H1968 occurs when Sending of E-mail FB is executed. Please tell me how to  treat it.

Category : 

Answer

"The number of characters specified in the input label: i_uBodyLength (number of characters in the body) is different from the number of characters in the body data of the input label: i_uBodyDataAddr (top address of the body data).
If you set the input label: i_uBodyLength (number of body characters) to "0," the number of body characters is set automatically. "

Product Name
FX5-ENET
Product Category
Network/Communication
Series
MELSEC iQ-F Series