• No : 44610
  • Release Date : 2024/11/28 16:11
  • Print

Regarding how to generate a false error

Does the FX5 CPU module have a function to generate false errors?

Category : 

Answer

There is no function to generate a false error.
For example, if operand (s2): divisor is set to "0" in the division command and the command is executed, error code: H3400 occurs.

Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module
Series
MELSEC iQ-F Series