Is there a way to compare multiple word devices?
It is possible to compare multiple word devices using the BKCMP_□ instruction.
*where □ is the comparison symbol.
Example:To compare 10 stores from D0 to D9 and from D100 to D109, write [BKCMP _□ D0 D100 D200 K10].
Comparison result is stored in 10 points from D200.