I am considering replacing the FX3U-128MR/ES, but the FX5U CPU module is limited to a 80 point lineup, so what kind of configuration should I make?
The FX5U CPU module has a lineup of up to 80 point.
The following configuration is recommended when replacing the FX3U-128MR/ES.
Recommended alternative (1)
・FX5U-80MR/ES + FX5-32ER/ES + FX5-16ER/ES
Recommended alternative (2)
・FX5UJ-60MR/ES + FX5-32ER/ES + FX5-32ER/ES + FX5-8EYR/ES