• No : 44618
  • Release Date : 2024/11/28 16:13
  • Print

Regarding how to change the averaging processing of FX5-4AD-ADP programmatically

In FX5-4AD-ADP averaging processing,is possible to change the number of counts for count averaging set in GX Works3 on the program?

Category : 

Answer

It is possible to change the number of counts for count averaging in a program.
Set the module parameter Basic settings to  "Set A/D conversion method" to Disable and change the number of counts for Count Average. After making the change, return to "Set A/D conversion method" to Enable.

For details, refer to the following manual.
MELSEC iQ-F FX5 User's Manual (Analog Control - CPU module built-in, Expansion adapter)

Product Name
FX5-4AD-ADP
Product Category
Analog
Series
MELSEC iQ-F Series