What is the maximum number of input/output points for the MX-F Model?
The maximum number of input/output points is 512.
The number of remote I/O points is not limited, but can be used within the specification range of each intelligent function module.
In addition, the MX-F Model does not have the number of I/O occupied points when the intelligent function module is connected, which was the case with the iQ-F series and the F series, so there is no need to consider it.