The CPU Module of the iQ-F series supports the built-in positioning function, but does the MX-F Model also support it?
The MX-F Model also supports the built-in positioning function.
The number of control axes is now 4, and PULSE/SIGN and CW/CCW are supported.
The maximum frequency is 200kpps.