What is the default IP address (factory default value) of the MX-F Model?
The MX-F Model has two built-in Ethernet ports.
In the following, the Ethernet port (P1) is referred to as P1 and the Ethernet port (P2) as P2.
*P2 selects Ethernet port or CC-Link IE TSN port when creating a new project in GX Works3.
The default IP address is as follows.
(1)When using P2 as an Ethernet port
P1 ⇒ CC-Link IE TSN port: 192.168.4.249
P2 ⇒ Ethernet port: 192.168.3.39
(2)Using P2 as a Port for CC-Link IE TSN
P1 ⇒ CC-Link IE TSN port: 192.168.4.249
P2 ⇒ CC-Link IE TSN port: same as P1.