• No : 45238
  • Release Date : 2025/10/22 16:51
  • Print

Window screen not displayed

The window screen does not display.

Category : 

Answer

If the window screen does not display, confirm the following. 
• The screen switching device for the window screen to be used is set in the screen design software.
• The value of the screen switching device is correct.

The screen corresponding to the value stored in [Screen Switching Device] is displayed as a window screen (overlap window, superimpose window, or dialog window). 
When the value of the screen switching device for the window screen to be used is 0, the window screen is closed.

◆ For GT Designer3 (GOT2000) Version 1
The number used to close the window screen can be set to a value other than 0. Change the setting in GT Designer3. 
[Common] - [GOT Environmental Setting] - [Screen Switching/Windows] - [Other Setting] - [Screen No. of the window screen to be hidden]
 

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (standard function)
Series
GOT1000 Series, GOT2000 Series, SoftGOT1000, SoftGOT2000, GOT3000 Series, SoftGOT3000