• No : 45264
  • Release Date : 2025/10/22 17:09
  • Print

How to capture the screen displayed on the GOT

Answer

The following methods are available to capture the screen displayed on the GOT. 
1. Use the preview function in the screen design software. 
2. Select [Project] → [Snap Shot] in GT Simulator3. 
3. Use the hard copy function on the GOT to store the image data on a data storage such as an SD memory card. 
4. Use the print function in the screen design software.

For details, refer to the screen design software manual.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GT Designer3, GOT function (standard function)
Series
GOT Screen Design Software, GOT2000 Series, GOT3000 Series