When connecting the MELSEC iQ-F series (FX5U, FX5UC, FX5UJ, or FX5S) via Ethernet, what should be set for Port No. in Connected Ethernet Controller Setting?
When connecting the MELSEC iQ-F series (FX5U, FX5UC, FX5UJ, or FX5S) via Ethernet, set Port No. in Connected Ethernet Controller Setting as shown in Table 2.
Select "FX5CPU" for the Unit Type field in Connected Ethernet Controller Setting.
◆ For GT Designer3 (GOT2000) Version 1
Figure 1: Port No. in Connected Ethernet Controller Setting

Table 2: Port No. to set for the controller in Connected Ethernet Controller Setting

○: Can be set, -: Cannot be set