• No : 45267
  • Release Date : 2025/10/22 17:10
  • Print

Open settings for connection to the built-in Ethernet port of the MELSEC iQ-R series

Answer

Open settings are required when the communication method of the GOTs is TCP for a single MELSEC iQ-R series controller (built-in Ethernet port). 
Configure the settings for [External Device Configuration] in GX Works3 for each connected GOT.

◆ For GX Works3
Go to the Navigation window then select → [Parameter] → [RnCPU] → [Module parameter] →
[Basic Settings] → [External Device Configuration] → [Detail settings] → [Ethernet configuration (built-in Ethernet port)]
Figure 1: When connecting two GOTs via TCP,

Open settings are not required when the communication method on the GOT side is UDP.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (communication)
Series
GOT2000 Series, SoftGOT2000, GOT3000 Series, SoftGOT3000