The touch switch is not displayed on the GOT.
If the touch switch is not displayed on the GOT, check the switch setting in the screen creation software.
◆ For GT Designer3 (GOT3000) Version 1
If the following settings are configured, the touch switch will not be displayed on the GOT.
1. In the [Basic Settings] tab, if [Lamp (Timing to change shape/text)] is set to [Bit-ON/OFF] or [Word Range], a device outside of the specified device range is set in the controller.
2. In the [Basic Settings] tab, [Shape] in [Style] is set to "None".