What causes slow screen switching?
Possible causes of slow screen switching are as follows:
• The incorrect communication driver is selected.
• When connected via Ethernet, a device with a duplicate IP address or station number is connected.
• The baud rate is incorrect for serial connection.
• When connected via Ethernet, a communication timeout has occurred on a channel.
• The execution cycle of background processes (scripts, logging, etc.) is short.