• No : 45284
  • Release Date : 2025/10/23 10:54
  • Print

How to enter a value using numerical keys placed on the same base screen without displaying the key window for numerical input

How do I enter a value using numerical keys placed on the same base screen without displaying the key window for numerical input?

Category : 

Answer

The method of entering a value using numerical keys placed on the same base screen without displaying the key window for numerical input is as follows: 
Configure the settings in the screen design software.

(Example) Place numerical keys next to the numerical input and enter a value using the keys.
 Figure 1

 ◆ For GT Designer3 (GOT3000) Version 1
 1. Place a numerical input on the base screen.
 2. Place numerical key. Using a template for the numeric keys
   (1) Select [Object] → [Select Library] → [Library List] to open the [Library] window.
   (2) Select the [System Library] tab in the [Library] window. Select [Object] under [System Library] then select [Numerical Key (Dec)] from the relevant folder*.
   *Select from [FA Metal_N], [FA Control_N], or [FA Plastic_N].
   (3) Numerical key templates will appear. Select a template then drag and drop it on the base screen.
 3. Setting a numerical input per project
   (1) Select [Common] → [GOT Environmental Setting] → [Key Window].
   (2) The [Environmental Setting] screen will appear. Select the [Advanced Setting] tab.
   (3) Configure each setting for [Key Window/Cursor Setting].
     • [Key Window]: Select [Hide].
     • [When operating conditions are not satisfied]: Select [Clear the key window and the cursor].
 4. Setting a numerical input per screen
   (1) Select the target screen to place the object on from the [Screen] tree, right-click the screen, and select [Screen Property].
   (2) Select the [Key Window Advanced Setting] tab in the [Screen Property] setting dialog.
   (3) Configure each setting for [Key Window/Cursor Setting].
     • [Prioritize screen setting over project setting]: Select this item.
     • [Key Window]: Select [Hide].
     • [When operating conditions are not satisfied]: Select [Clear the key window and the cursor].

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (numerical display/text display), GOT function (numerical input/text input), GT Designer3
Series
GOT3000 Series, GOT Screen Design Software, SoftGOT3000