• No : 45291
  • Release Date : 2025/10/22 17:12
  • Print

How to display integer values written to the PLC as real numbers (with decimal points) on the GOT

How do I display integer values written to the PLC as real numbers (with decimal points) on the GOT?

Category : 

Answer

Use the automatic decimal place adjustment function to display the integer value written to the PLC as a real number on the numerical display on the GOT. 
Configure the settings in the screen design software.

◆ For GT Designer3 (GOT2000) Version 1
Configure the following settings.

If the value 123 is written to the specified device (D0), 1.23 is displayed on the numerical input object. 
To display the device value 123 as 123.00, deselect the automatic decimal place adjustment function.

For details, refer to the screen design software manual.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (numerical input/text input)
Series
GOT1000 Series, GOT2000 Series, GOT3000 Series, GOT Screen Design Software, SoftGOT2000, SoftGOT3000