• No : 45293
  • Release Date : 2025/10/22 17:12
  • Print

Setting the PLC station number when connecting the GOT to the PLC via Ethernet

Answer

The following shows how to set the PLC station number when connecting the GOT to the PLC via Ethernet. 
Configure the settings in the screen design software.

◆ For GT Designer3 (GOT2000) Version 1
[Common] → [Controller Setting] → [Connected Ethernet Controller Setting]
Ensure that [GOT Station] and [Station] are not duplicated in Connected Ethernet Controller Setting. 
Figure 1

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (communication)
Series
GOT3000 Series, GOT2000 Series, SoftGOT3000, SoftGOT2000