• No : 45295
  • Release Date : 2025/10/22 17:12
  • Print

Switching the GOT screen from being displayed to hidden

Can the GOT screen be switched from being displayed to hidden?

Category : 

Answer

Switching is enabled by using the system information (read device). 
The GOT screen can be displayed/hidden by turning ON/OFF the Forced Screen Saver Enable signal (System signal 1-1.b1).

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (standard function)
Series
GOT1000 Series, GOT2000 Series, GOT3000 Series, SoftGOT1000, SoftGOT2000, SoftGOT3000