• No : 45299
  • Release Date : 2025/10/22 17:13
  • Print

Specifying the display position of the key window

How do I specify the display position of the key window in the screen design software?

Category : 

Answer

Specify the display position of the key window in the screen design software as follows.

◆ GT Designer3 (GOT3000) Version 1, GT Designer3 (GOT2000) Version 1
Configure the following settings to specify the display position of the key window.
1. Select [Common] → [GOT Environmental Setting] → [Key Window]. Then in the [Advanced Setting] tab select [Not move] or [To the four corners of the screen] for [Key Window Position Correction] under [Key Window/Cursor Movement].
2. Select [Object] → [Window Position] → [Key Window].
* The mouse cursor will change to a [+]. 
3. Click the mouse at a position in the upper left corner where you want to display the key window.

◆ GT Designer3 for the (GOT1000) Version 1
Configure the following settings to specify the display position of the key window. 
1. Select [Object] → [Window Position] → [Key Window].
* The mouse cursor will change to a [+]. 
2. Click the mouse at a position in the upper left corner where you want to display the key window.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (standard function)
Series
GOT1000 Series, GOT2000 Series, GOT3000 Series, GOT Screen Design Software, SoftGOT2000, SoftGOT3000