What is the maximum number of years that the clock function of the FX5 CPU module can handle? Also, what happens if the number of years is exceeded?
The maximum number of years of the clock function is 2079 years.
If it exceeds the maximum number of years, it will be fixed at 23:59:59 on December 31, 2079.