• No : 45482
  • Release Date : 2025/11/12 13:55
  • Print

Regarding the expansion of modules after the bus conversion module

The FX3 series module is added to the rear stage of the bus conversion module (FX5-CNV-BUS, FX5-CNV-BUSC). Is it possible to add an iQ-F series module to the later stage?

Category : 

Answer

It is not possible to add an iQ-F series module after the bus conversion module. When adding an iQ-F series module, add it in the front stage of the bus conversion module.

Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module
Series
MELSEC iQ-F Series