• No : 45483
  • Release Date : 2025/11/12 13:55
  • Print

Regarding EtherNet/IP communication function for FX5-EIP

What EtherNet/IP communication functions does the FX5-EIP support?

Category : 

Answer

The following EtherNet/IP communication functions are supported by the FX5-EIP.
・Cyclic communication function ⇒Class1 instance communication/tag communication
・Message communication function (client) ⇒Class3 instance communication/tag communication, UCMM instance communication/tag communication
・Message communication function (server) ⇒Class3 instance communication/tag communication, UCMM instance communication/tag communication

Product Name
FX5-EIP
Product Category
Network/Communication
Series
MELSEC iQ-F Series