How can I check the connection status and input/output data from GX Works3 to FX5-EIP?
This can be checked by monitoring the corresponding buffer memory from the Register to Intelligent Function Module Monitor.
From [Parameter] - [Module Information] in the navigation window of GX Works3, right-click FX5-EIP and select "Register to Intelligent Function Module Monitor."