- No : 21344
- Release Date : 2018/08/22 16:27
-
Print
Applied terminal
When connecting a potentiometer with the terminals 10, 2, and 5 of the inverter, do I have to use the shielded cable?
- Category :
-
Answer
As described in the instruction manual, use the shielded cable or twisted cable to avoid the influence of noises.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700