- No : 21724
- Release Date : 2018/08/22 16:29
- 
          
              Print
          
        
 
Electromagnetic contactor
    
      Is it possible to avoid open/close surges of the electromagnetic contactor by setting the inverter parameters?  
    
  
    - Category : 
- 
      
    
 
    Answer
  
    It cannot be avoided by using parameters.  
  
    
      
        - Product Name
- Inverter, magnet motor drive
        - Product Category
- Inverter
        - Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700