- No : 21849
- Release Date : 2018/08/22 16:29
-
Print
External operation
While externally operating the conveyor, turn of the external potentiometer does not match the actual speed.
Can I adjust them?
- Category :
-
Answer
The inverter has the calibration function.
Use Pr.125 (Terminal 2 frequency setting gain frequency) and Pr.C4 (Terminal 2 frequency setting gain) for calibration.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700