• No : 21849
  • Release Date : 2018/08/22 16:29
  • Print

External operation

While externally operating the conveyor, turn of the external potentiometer does not match the actual speed.
Can I adjust them?
Category : 

Answer

The inverter has the calibration function.
Use Pr.125 (Terminal 2 frequency setting gain frequency) and Pr.C4 (Terminal 2 frequency setting gain) for calibration.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700