• No : 23546
  • Release Date : 2018/09/14 15:07
  • Print

Improved UV resistance of the rugged model

Answer

The UV resistance of the rugged model has been improved in two points.
The UV cutoff environmental protection sheet (not replaceable) is used on the GOT front face.
This reduces degradation of the touch panel and display.
Changing the material of the GOT front face from resin to aluminum reduces degradation of the front panel.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Rugged model
Series
GOT2000 Series