- No : 23549
- Release Date : 2018/09/14 15:07
-
Print
CC-Link IE Field Network Basic connection of the rugged model
Does the rugged model support the CC-Link IE Field Network Basic connection?
- Category :
-
Answer
The rugged model supports the CC-Link IE Field Network Basic connection.
Both Ethernet interface Port1 and Port2 are connectable to controllers that support the Ethernet and CC-Link IE Field Network Basic connections.
The GOT2000 series operates as a slave station and is connectable to controllers that operate as a master station.
(Supported by the RJ-45 connector (Port1, Port2))
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model, GOT function (communication)
- Series
- GOT2000 Series