FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Setting values of the FR-F800 when replaced with the FR-F400
FAQ
Setting values of the FR-F800 when replaced with the FR-F400
Is the Pr.10 (PWM mode) setting value of the FR-F400 and the Pr.72 (PWM frequency selection) one of the FR-F800 to be the same?
- Category :
Answer
The performance and noise countermeasure were improved and the initial value is set to "8". Try with the initial value "2" first. If the noise is distracting, increase the value gradually.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800