FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A8NC
FAQ
FR-A8NC
The rotations per minute command is sent from CC-Link by Pr.144 = 108. When 422 rpm is sent, the theoretical value monitored as the setting frequency by the communication is 28.133333..Hz. Is this value rounded up or off?
- Category :
Answer
Two digits after the decimal point are rounded off. 28.139 Hz is rounded down to 28.13 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- Option