FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > TH3 terminal of the MT-BR5
FAQ
TH3 terminal of the MT-BR5
There are TH1, TH2, TH3, and E terminals on the control circuit terminal block. What is the TH3 used for?
- Category :
Answer
The resistor unit MT-BR5 manufactured in February 2016 or later has output terminal TH3 (NC contact) as a fault output terminal.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Option
- Series
- Option