FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Safety stop function of the FR-E700/FR-D700
FAQ
Safety stop function of the FR-E700/FR-D700
When the safety stop function is used, how many inverters can be connected?
- Category :
Answer
Up to two.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-D700, FR-E700