FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > S-shape acceleration/deceleration of the FR-D700
FAQ
S-shape acceleration/deceleration of the FR-D700
When Pr.29 (Acceleration/deceleration pattern selection) is set as S-shape acceleration/deceleration, does the inflection point of S-shape change from Pr.3 to Pr.84 under General-purpose magnetic flux vector control?
- Category :
Answer
It does not change even when General-purpose magnetic flux vector control is performed. Pr.3 is the inflection point of the S-shape.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-D700