FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Options > Leakage current of the FR-BIF
FAQ
Leakage current of the FR-BIF
In the Instruction Manual, it is described that the leakage current at the star connection is 4 mA. How much is the leakage current at the delta connection?
- Category :
Answer
For the 200 V type, the leakage current at the delta connection is 5 mA. For the 400 V type, it is 10 mA.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Option
- Series
- Option