FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FR Configurator2
FAQ
FR Configurator2
The option of the FR-A8TP is enabled by FR Configurator2, but Vector control cannot be selected in the motor setting. Why?
- Category :
Answer
Vector control cannot be selected unless Pr.862 is set to 1. Only the first motor is supported in the motor setting of FR Configurator2.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Engineering software
- Series
- FR Configurator2