FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > STOP function of the FR-A800
FAQ
STOP function of the FR-A800
Is the self-holding of the STOP function released by the OH signal (External thermal relay input)?
- Category :
Answer
No, it is not. It is released by the inverter reset that releases E.OHT.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800