FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Engineering Software > FR Configurator2
FAQ
FR Configurator2
In FR Configurator2, the option of the FR-A8TP is enabled. Why Vector control cannot be selected in the motor setting?
- Category :
Answer
Vector control cannot be selected unless Pr.862 is set to 1. Only the first motor is supported in the motor setting of FR Configurator2.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Engineering software
- Series
- FR Configurator2