FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Engineering Software > High speed sampling of FR Configurator2
FAQ
High speed sampling of FR Configurator2
Is the high speed sampling of the graph available when the FR-A800-E is connected via the Ethernet?
- Category :
Answer
High speed sampling is not available. Only the normal sampling is available.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Engineering software
- Series
- FR Configurator2