FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Circuit type of the FR-D700W/FR-E700W in the harmonics suppression guideline
FAQ
Circuit type of the FR-D700W/FR-E700W in the harmonics suppression guideline
What circuit type is the FR-D700W/FR-E700W in the harmonics suppression guideline?
- Category :
Answer
It is single-phase bridge (smoothing capacitor, double voltage rectification).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-D700, FR-E700