FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A8TR
FAQ
FR-A8TR
As the restriction of the FR-A8TR, it is described that the terminals +24, 10E, 4, and STOP are unavailable when the FR-A8NC is used. What is the reason for that?
- Category :
Answer
Because when the FR-A8NC and FR-A8TR are used together, the wiring to the terminals becomes physically difficult.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- Option