FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800-R2R
FAQ
FR-A800-R2R
When the winding diameter calculation is performed in the thickness method by using the motor with encoder, can I use only winding diameter compensation under the normal speed control?
- Category :
Answer
It is possible when the dancer control and tension sensor feedback speed control is used and the PID calculation is turned OFF. Because the PID compensation cannot be used and no compensation is performed for disturbance, the accuracy decreases.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800-R2R