FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800-R2R
FAQ
FR-A800-R2R
The normal speed control is performed when X114 is turned OFF. Can I use the second terminal as a frequency setting value when Pr.361 is set? I want to use the second terminal for the line speed command and frequency setting in the normal mode.
- Category :
Answer
If Pr.361 = 0, the second terminal can be used as the line speed command when X114 is ON, and as the frequency setting value when X114 is OFF. If Pr.361 = 3, the second terminal does not function as the frequency setting when X114 is OFF.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800-R2R