FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Load characteristics fault detection
FAQ
Load characteristics fault detection
When Pr.1480 (Load characteristics measurement mode) is set to "1" with the load characteristics fault function, the load characteristics load reference is set to Pr.1481 to 1485. To what is this percentage compared?
- Category :
Answer
It is based on the motor rated torque.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-F800