FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Terminal 2 input selector switch when the PTC thermistor is connected
FAQ
Terminal 2 input selector switch when the PTC thermistor is connected
Does the DIP switch of the second terminal of the PTC thermistor (10 to 2 terminals) operate normally even after it is switched from V to I?
- Category :
Answer
When the DIP switch is changed to I, it does not operate normally because the internal resistance changes.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800