FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Monitoring function of the FR-A800-R2R
FAQ
Monitoring function of the FR-A800-R2R
Can I monitor Pr.52 = 26: Line speed command, 27: Actual line speed, and 31: Line speed pulse monitor while the operation is stopping? Is there any requirement for the monitor indicator?
- Category :
Answer
Line speed command and Line speed pulse monitor can be monitored while the operation is stopping. Actual line speed monitor becomes "0" while the operation is stopping. Line speed pulse monitor can be monitored while the operation is stopping only when Pr.362 = 1, 2, or 7. When Pr.361 = 1, 2, or 7 and Pr.362 = 1, 2, or 7, the input of Pr.361 is disabled as the functions are duplicated.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800 Plus