FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR Configurator2
FAQ
FR Configurator2
Is there any function to display the parameters changed from the initial value?
- Category :
Answer
Yes, the changed parameters can be displayed with the verification function. Select Parameter list → Verification → Initial value.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Engineering software
- Series
- FR Configurator2