FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A8NC
FAQ
FR-A8NC
When the torque limit is input via the CC-Link, what happens if a negative value is written to the torque limit? For example, what happens when -100% is written?
- Category :
Answer
The torque limit setting is defined as an absolute value. Thus, when -100% is written to the torque limit, the torque is limited at 100%.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- Option